Reliable ESD and surge protection in smaller footprint; wide product portfolio
March 2019 – TDK’s EPCOS SMD multilayer varistors provide reliable surge and ESD protection for sensitive components and are now available from TTI, Inc., a world leading specialist distributor of electronic components. Offering high reliability and long-term stability they are ideal for applications such as smart home and security devices.
EPCOS SMD multilayer varistors (MLVs, CeraDiode® and CTVS®) provide surge current ratings comparable to those of disk varistors as alternatives to TVS diodes, but offer the advantages of enabling smaller and more robust designs. The EPCOS B72*T* series of SMD multilayer varistors are available in a wide range of types and in compact case sizes 0201 to 2220. Features include no derating up to +125 °C and low leakage current. The components are UL compliant, with ESD accredited to IEC 6100-4-2 and surge accredited to IEC 60060-4-5.
Applications for the B72*T* series include providing ESD protection in NFC (nearfield communication) and interfaces (CAN, Ethernet, USB 2.0, USB 3.0, and bus systems). They are also an excellent fit to give high energy transient/surge protection for thermostats, and Power over Ethernet plus multiple security applications: detection (motion, vibration, opening, breakage of glass, access control, burglar, smoke, heat and water alarms); sender (manual pull stations, emergency call senders, assault senders) and communication modules (ISDN, CSM, info modules, control panels).
About TTI, Inc.
TTI, Inc. a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains two million cubic feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and Symmetry Electronics, TTI employs over 5,400 employees and is represented in over 100 locations throughout Europe, North America and Asia. For more information about TTI, visit www.ttieurope.com
For further information contact:
TTI, Inc.
T: +49 8142 6680 – 0
E-mail: sales@de.ttiinc.com
For Press Information contact:
TTI, Inc.
Geoff Breed
VP Marketing - Europe
T: +49 8142 6680 – 308
F: +49 8142 6680 – 9308
E-mail: Geoff.Breed@uk.ttiinc.com
Or
Anna Johnston
Senior Account Director, BWW Communications
T: +44 1491 636393
F: +44 1491 636383
E-mail: anna.johnston@bwwcomms.com