TTI Europe
TTI Europe - The World's Leading Passive and Connector Specialist
Download PDF
PDF
www.ttieurope.com
UK DE FR IT ES
  TTI News Update
June 2008
www.ttieurope.com
 
TTI Links:
 
· TTI Home
· About TTI
· Downloads

 

Supplier Microsites:
· Amphenol
· AVX
· Bourns
· FCI
· Kemet
· Molex
· Murata
· Phoenix
  Contact
· TT Electronics
· Tyco
· Vishay
· Yageo

 

Lead Free:

 

TTI Linecard :

 

Bourns introduces applications for RF Power Resistors

Isolators, Combiners, Dividers, Couplers are sub components within transmitter stages of wireless equipment. These subcomponents require RF Power Resistors, usually 50 Ohms or 100 Ohms to terminate unused ports to ground or to provide balance between different phases. Normally these resistors never receive any power during the operation of the subcomponent.

To read more click here...

KEMET announces the launch of it's new Space Grade Tantalum chip series.

KEMET’s Space Grade series of capacitors are designed for use by military/aerospace customers in high reliability space applications. This series meets the requirements of MIL-PRF-55365 as well as applicable requirements of MIL-STD-1580. These capacitors incorporate an intensive testing and screening protocol which is customizable depending upon customers’ specific needs.

To read more click here...

Nichicon introduces CONDUCTIVE POLYMER ALUMINUM SOLID ELECTROLYTIC CAPACITORS

The construction and function of a Polymer type Capacitor is basically the same as an Aluminum Capacitor. The main difference between the two technologies is the electrolyte material. Liquid electrolyte is used In Al-Capacitors, whereas in Polymer Capacitors solid electrolyte is used.

To read more click here...

Molex dual positive lock CLIK-Mate 2.00mm SMT connectors offer secure mating retention and electrical contact in a broad range of applications

Molex Incorporated introduces a new series of 2.00mm (.079") pitch SMT wire-to-board connectors designed for applications that require secure electrical contact. The CLIK-Mate™ connector features a positive locking mechanism that provides an audible click, so operators know when it is fully mated.

To read more click here...

WIMA Double Layer Capacitors with Capacitances up to 3000 F

To read more click here...

Tyco Electronics and TTI announce EMEA partnership on connectors for the Aerospace, Defence and Marine market.

To read more click here...

Offers Real-Time X-Ray Capability

To read more click here...
To register for a monthly newsletter e-mailed to you or for more information on TTI visit our website: http://www.ttieurope.com