TTI_VAD_Visual

November 2012 – TTI, Inc., the world’s largest specialist distributor of passive, discrete, connector and electromechanical components, has announced new capabilities offered by its European connector assembly facility, located at the company’s European headquarters outside of Munich, Germany.  TTI can now offer a comprehensive service covering Amphenol and Souriau circular connector types and is QPL Certified for both manufacturers’ products.

Amphenol’s MIL-DTL-38999 Series I & III connectors are available in all types of Aluminium shells, sizes and layouts with a choice of PC tail, coax, power and signal contacts. Over 1500 component parts are held in stock and platings available include Olive Drab Cadmium and Electroless Nickel. Devices can be supplied to meet the French HE308 standard (LJT 38999 Series I) or to Amphenol’s approved commercial grade (TVxx). TTI can also assemble Amphenol’s MIL-C-26482 PT/451 Series connectors

Souriau MIL-DTL-38999 Series I Aluminium connectors are available with Olive Green Cadmium and Nickel Platings. MIL-DTL-38999 Series III devices can also feature Black Zinc Nickel plating which is ROHS compliant, or Green Zinc Cobalt  - a commercial plating. Devices are also available with Composite and Stainless Steel shells.

Comments Thilo Pelosato, Marketing Director, Europe – Military, Aero and Space, TTI, Inc.: “We see a growing market demand for Composite and Power connectors, so we have strengthened our capabilities in this area. Customers are also looking to reduce size and weight so we have introduced some smaller product options. As well as the traditional defence and aerospace sectors, electric vehicle, marine and industrial applications are also performing well, so we have added to our expertise in these areas to support our customers.

“Our microsites, www.ttieurope.com/38999 and www.ttieurope.com/page/mil-dtl-26482 detail our capabilities and product offerings and include data-sheets and a comprehensive part number search engine to help designers find the parts they need.”