Featured Suppliers: Molex, Murata, Panasonic, Phoenix Contact, TE Connectivity, Vishay

November 2016
 



Dear Transportation Customer,

With the Commercial Vehicle market set to expand, TTI continues to invest in new products to serve customers in this diverse market. In order to keep our customers up to date, our new Transportation catalogue features additional 60 pages of products compared to the original version from just two years ago. Use the link below to see the digital version of our Connector, E-Mech, Passive, Discrete and Sensor technologies offerings.

Some of the new products featured in the catalogue include: the Molex ML-XT products which offer improved sealing performance compared to de-facto standard products in the industry; higher voltage contactors from TE Connectivity that support currents up to 600A; Inclinometers from Murata which help determine the 3D position of agriculture and construction equipment when they are operating in rough outdoor environments; and Phoenix Contact's new AC vehicle connectors which rely on robust and high-quality materials, as well as on a uniform plug design. From our passive suppliers, we have expanded our portfolio of Hybrid capacitors with Panasonic and of Surface Mount PAR® Transient Voltage Suppressors from Vishay.

For more information about our suppliers’ solutions, visit www.ttieurope.com

Best regards,

Dermot Byrne - Director Industry Marketing Transportation


Molex

ML-XT™ Sealed Connection System

The rugged ML-XT™ connection system with market leading high-performance seal technology is a cost competitive solution offering superior reliability for critical vehicle-wiring applications in harsh environments.

Amphenol POWERLOK


Murata

Inclinometers

Murata inclination sensors are an optimum choice for high accuracy leveling and inclination measurement instruments. The highest accuracy is available with SCA103T series that use differential measurement principle to compensate all common mode error and noise effects.

SMCAN 24A/B

Panasonic

New Hybrid ZK Series

ZK series optimizes designs with regards to performance, cost and weight, low leakage current, long life and low ESR values.

Molex ML-XT

Phoenix Contact

The Trendsetter - Vehicle Connectors for E-Mobility
Phoenix Contact offers the complete range of charging connectors from a single source: Type 1, Type 2 and GB/T standard.

SVK3

TE Connectivity

KILOVAC Contactors

TE Connectivity's KILOVAC Contactors offer low and stable contact resistance over relay life as well as high resistance to shock, vibration and temperature extremes.

Phoenix Contact AC Chargers and Controllers

Vishay

Surface Mount PAR® Transient Voltage Suppressors

TPC11CA to TPC36CA. Industry-First 1500W Bidirectional PAR® TVS in Low-Profile SMPC (TO-277A) Package.

TE EVC 250

Latest News...

  Transportation Brochure
  See TTI's product offering now

  TTI's New Line Card
  See TTI's Updated Line Card

europe-mil-news-learn-more

europe-mil-news-learn-more

   
TTI, Inc. - Never Short on Solutions
This email was sent by: TTI, Inc.
Ganghoferstr. 34 Maisach-Gernlinden, Bavaria, 82216, Germany
Tel: +49 8142 6680 - 0 l Email: sales@de.ttiinc.com
Copyright ©2015 TTI, Inc. All Rights Reserved.