Transportation Newsletter
Dear Transportation Customer,
 
The commercial vehicle market is going through a period of dynamic change. Manufacturers are starting to develop alternative drive systems to limit vehicle emissions and optimise fuel economy. They are also investing in enhanced telematics systems to enable route optimization and ensure better capacity utilization. To prepare for these developments, TTI is adding both, new franchises and new supplier products that offer solutions to the needs of the market.
 
In recent months, TTI has expanded its franchise relationship with ITT Cannon to offer its range of rugged connector solutions across the full EMEA region. We have also invested in stock of Delphi’s AK class connector products, KOA’s latest current sense resistors and Bourns high power inductors series to meet the needs of manufacturers of electric and hybrid drive systems. Furthermore, by stocking Molex new Valuseal product, AICC USB Type C Gen 1 connectors and Vishay’s optical sensors, TTI can support manufacturers in the development of new telematics and body electronic systems for their next generation vehicles. For more details on these new developments, please click on the links below.
 
For more information about our suppliers' solutions, visit www.ttieurope.com.
 
Best regards,
 
 
Dermot Byrne - Director Industry Marketing Transportation
AVX Automotive Varistors
Amphenol ICC
USB 3.1 TYPE C CONNECTORS
Amphenol ICC USB 3.1 Type C Gen 1 and 2 Receptacle Connectors offer a small form factor and a reversible design that enables quick and easy connections no matter which way they are inserted.
 
Learn More
JST Automotive Connectors - AIT & AIT II Series
Bourns
BOURNS® SMD High Current Shielded Power Inductors
The models include the SRP1038A, SRP1238A, SRP1245A, SRP1265A and SRP7028A power inductors.
 
Learn More
 
Littelfuse Automotive Surface Mount Load Dump TVS
Delphi
AK Class 4 Connectors
Product designed for power conversion applications - primarily battery and inverter connections.
 
Learn More
 
Molex Multimedia Module (CCP)
ITT Cannon
APD Connectors & Modular Interface
The APD Series is a lightweight, cost effective plastic connector line that is designed in accordance to ISO 15170.
 
Learn More
Murata Lead Type MLCCs for 200�C Automobile Use
KOA
Metal Plate Power Shunts - Automotive
For high current applications, KOA has now expanded its existing power shunt series by adding the new PSJ2/PSL2 (2 terminals) and PSG4/PSF4 (4 terminals) series.
 
 
Learn More
 
 
Panasonic Power Inductor Metal Composite Type
Molex
ValuSeal Wire-to-Wire Connector
Achieve industry-leading cost efficiencies and IP65 sealing protection with the innovative, one-piece ValuSeal Wire-to-Wire Connector, ideal for consumer, non-automotive transportation and industrial applications.
 
 
Learn More
Yageo Thin Film Automotive Resistors
Vishay
VCNL4035X01 Optical Sensor
VCNL4035X01 integrates a proximity sensor (PS), ambient light sensor (ALS), a muxx, and a driver for up to 3 external IREDs / LEDs into one small package.
Learn More
 
 
 
Latest News...
 
TTI Line Card
Line Card
See TTI's product offering now
Learn More
TTI Automotive and Transportation Line Card
Automotive & Transportation Catalogue
See TTI's product offering now
Learn More
This email was sent by: TTI Europe
TTI Europe | Ganghoferstr. 34 | Maisach-Gernlinden | Bavaria 82216 | Germany