12/17/2015 //
November sales for Taiwan-listed companies (many of which manufacture in China) were just released:
Source: Company financial reports aggregated by Custer Consulting Group
SEMI reported that worldwide semiconductor manufacturing equipment billings reached US$9.6 billion in the third quarter of 2015. The billings figure is 3% higher than the second quarter of 2015 and 9% higher than the same quarter a year ago. The data is gathered jointly with the Semiconductor Equipment Association of Japan (SEAJ) from over 100 global equipment companies that provide data on a monthly basis.
Worldwide semiconductor equipment bookings were $8.7 billion in the third quarter of 2015. The figure is 7% lower than the same quarter a year ago and 14% lower than the bookings figure for the second quarter of 2015.
Source: www.semi.org
The total production value of electronic systems is forecast to decrease 2% in 2015 to an estimated $1,423 billion, marking only the fourth time in history that the systems market registers a decline (previous years were 2001, 2002, and 2009). Total electronic system sales are forecast to reach $1,614 billion in 2019, which represents a compound annual growth rate (CAGR) of 2.1% from $1,454 billion in 2014. Chart 13 compares the relative market sizes and projected growth rates of nine major systems segments covered in IC Insights’ recently released 2016 edition of its IC Market Drivers report. These nine market categories represented approximately 70% of the estimated total production value of all electronic systems in 2015.
Among individual end-use systems covered in detail in the 2016 IC Market Drivers report, cellphones expanded their lead over standard personal computers (desktops and notebooks) as the largest electronic systems market in 2015 after overtaking PCs for the first time in 2013.
Cellphones accounted for 18% of total electronics systems sales ($262.2 billion) versus about 13% for standard PCs ($187.4 billion) in 2015. Cellular phone sales are projected to rise by a CAGR of 2.9% in the 2014-2019 period, while standard PC revenues are expected to slump by an annual rate of -1.7%, partly due to longer upgrade cycles for standard PCs, the influx of tablet computers into the mix of computing platforms, and the growing use of smartphones to access the Internet.
The Internet of Things system market is forecast to show the highest average annual growth rate (21%) through 2019. Aside from this one high-flying market, however, no other system category is forecast to average annual growth of more than 7%. In fact, the standard PC, tablet, and game console system markets are forecast to decline through 2019.
Source: www.icinsights.com
Global automotive PCB market size was around US$ 4.96 billion in 2014, and is expected to grow by 6.5% to US$ 5.28 billion in 2015.
This compares to an overall global PCB market scale of roughly US$ 59.6 billion in 2014 and an estimated growth of 0.8% in 2015. Automotive PCB is the fastest-growing field in PCB industry, and will sustain the momentum until at least 2019.
In automotive PCB field, powertrain holds the largest proportion, about 32% for the time being, including mainly Engine Control Unit, Starter, Alternator, Transmission Control, Fuel Injection, and Power Steering. For xEV, complexity, high voltage, high current and high temperature of Inverter and Converter pose extremely high requirements on PCB.
Powertrain seizes over 50%, followed by Body with about 25% (primarily Lighting, HVAC, Power Door and Seat, Keyless, and TPMS). LED lighting, which enjoys a high share, is highly demanding on PCB, usually adopting MCPCB (Metal Core PCB). Thirdly, Safety systems, consisting mainly of ADAS, ABS, and Airbag, make up about 22%. The last is Cockpit systems, mainly covering Instrument Display and Infotainment.
Automotive PCB has exceedingly high requirement on reliability, creating the biggest threshold. Recall system in automobile industry requires makers to take risks of faulty products. As small makers cannot afford this, they are usually ruled out. Challenges for automotive PCB include reliability, high temperature, high frequency, and high current.
PCBs in automotive engine and gearbox need to withstand high temperature above 150 ℃, so ceramic substrates must be used, for ceramic multilayer substrate contains mainly alumina (Al2O3) and aluminum nitride (AlN). High temperature co-fired ceramic (HTCC) PCB is usually sintered at temperature of over 1600 ℃ and the conductor is high-melting point tungsten or molybdenum, which can be sintered together at the same time.
Japanese Murata puts forward low temperature co-fired ceramic (LTCC), which finds few applications. Ceramic substrates are mostly supplied by Japanese KYOCERA and U.S. Rogers. PCBs used by European and U.S. carmakers are largely provided by German Schweizer, Duwel, and Wurth, and U.S. TTM. Japanese carmakers are mainly served by CMK and Meiko.
Automotive safety systems, especially ABS, generally adopt MCPCB (Metal Core PCB). Automotive ADAS needs to use a large quantity of radar which finds shipment of 19 million sets in 2014 and is expected to reach 96 million sets in 2020. In this case, high-frequency PCB will be employed. The PCB usually needs PTFE ceramic and can only be done by the companies (mainly from U.S. Europe and Japan) that are very experienced in RF. xEV is developing rapidly, especially after the outbreak of scandal over VW cheating pollution emissions tests.
Supply of cockpit PCBs are almost taken on by Taiwanese companies. HDI may be needed, as Infotainment becomes more complicated and the size of screen larger. Moreover, the number of automotive displays used also increases, like BMW 7 series using up to 7 displays for each vehicle. All these factors fuel a robust market.
Despite seeing growth in third quarter worldwide PC shipments, the PC supply chain is still conservative about demand from the fourth quarter to the first half of 2016 as most PC demand in the fourth quarter comes from price-cut promotions with the only exception being Apple's Mac-series products.
Source: www.digitimes.com
According to the International Data Corporation (IDC) the total security appliance market showed positive growth in both vendor revenue and unit shipments for the third quarter of 2015 (3Q’15). Worldwide vendor revenues increased 9.6% year-over-year to $2.7 billion, and shipments grew 9.7% year-over-year to a total of 585,282 units. The sub-market with the strongest year-over-year growth was Unified Threat Management (UTM) with a 17.8% increase in revenues. The Firewall, Intrusion Detection and Prevention, and Content Management sub-markets also continued on a growth trajectory with 6.7%, 6.6% and 1.3% year-over-year growth respectively. The Virtual Private Network (VPN) sub-market was the only one showing a year-over-year decline (-16.3%).
"Security products remain a growing industry as threats continue to plague companies. Over the past year the threat landscape has increased, leading to growth globally as no country is free from attacks," said Elizabeth Corr, Research Analyst, Security Products at IDC. “This growth is reflected in the top 5 vendors growing a combined 9.4% year-over-year."
Source: www.idc.com
Walt Custer is an industry analyst focused on the global electronics industry. Prior to forming Custer Consulting Group he was Vice President of Marketing and Sales for Morton Electronic Materials, a global supplier of specialty chemicals and process equipment for the PCB industry.
Custer has been a member of the IPC trade organization since 1975 where he received both the President's and the Raymond E. Pritchard Hall of Fame Awards. He is currently a member of the IPC Executive Market & Technology Steering Committee. Custer is also a Director of the EIPC European PCB trade organization.
He authors regular “Market Outlook” columns for Global SMT & Packaging magazine, the Journal of the HKPCA and the TTI MarketEYE website.