06/22/2017 //
The Internet of Things is not only driving the electronic component market, but it’s also influencing the direction design/development kits are taking. While passives and connectors are changing to meet the new demands of IoT projects (for example many IoT nodes need capacitors for coupling, decoupling and filtering), manufacturers also are being asked to deliver smaller packages that deliver the same capacitance or resistance as their former larger versions along with excellent reliability and a high Mean Time To Failure (MTTF). A similar trend can be found in connectors targeting IoT applications. USB-C devices, for instance, enable engineers to create wearables with fewer connecting cables.
Given all of that, it should not be surprising to find suppliers of passives trying to simplify matters for engineers by providing a range of components and solutions for a large number of IoT applications, including wearable devices (e.g., health and fitness accessories), smart homes (automated lighting and heating), industrial automation (predictive maintenance) and connected and semi-autonomous cars.
One harbinger of the sort of thing engineers can expect in support of these efforts was the recent release of a new passive component IoT design kit from AVX.
Let’s take a closer look.
The new Passive Components for the Internet of Things Design Kit (Part Number: KIT-IOT) allows engineers to quickly identify effective solutions for IoT devices with widely varying requirements for power, data processing speed, form factor, and price, among other specifications. It is comprised of a broad sampling of passive components suited for use in the three primary IoT device networks: input voltage filtering and decoupling, timing device, and output impedance RF matching.
Including ceramic capacitors, inductors and crystal devices the kit aims to deliver all the passive components needed for application development in one package, greatly reducing the amount of time and effort required by designers to procure sample-use components.
Component solutions ideal for use in the input voltage filtering and decoupling networks of IoT devices represented in the Passive IoT Design Kit include:
As the IoT market continues to grow, companies with less than optimal experience in RF design are seeking to add wireless connectivity to existing products, or design new ones targeting the IoT. To relieve some of the common pain points in RF design for IoT devices AVX includes solutions for the output impedance matching networks of IoT RF antennas in the kit:
The kit also includes crystal components that are useful in IoT applications requiring tight frequency stability, such as in clock management, MCUs, application processors, and wireless applications such as Bluetooth low energy (BLE), WIFI, and GPS. The crystal units (CX2016DB and ST3215SB series) are from Kyocera (AVX is a member of the Kyocera group). The kit also contains the U series of RF ceramic capacitors for crystal unit loading.
Murray Slovick is Editorial Director of Intelligent TechContent, an editorial services company that produces technical articles, white papers and social media posts for clients in the semiconductor/electronic design industry. Trained as an engineer, he has more than 20 years of experience as chief editor of award-winning publications covering various aspects of consumer electronics and semiconductor technology. He previously was Editorial Director at Hearst Business Media where he was responsible for the online and print content of Electronic Products, among other properties in the U.S. and China. He has also served as Executive Editor at CMP’s eeProductCenter and spent a decade as editor-in-chief of the IEEE flagship publication Spectrum.