12/13/2016 //
(Messee Munchen, Germany) KEMET Electronics Corporation unveiled their much anticipated line of automotive varistors at the Electronica 2016 fairgrounds in Messee Munchen Germany this month (November 2016), and officially entered the $5 billion* global market for circuit protection components. Traditionally KEMET has been a global manufacturer of capacitors, dominating the world market for tantalum and plastic film capacitors; and competing in specialty segments of the ceramic and aluminum electrolytic capacitor markets worldwide, moreover, with the acquisition of NEC Corporation’s Tokin Subsidiary, a major manufacturer of components other than capacitors, KEMET has accessed new markets in a variety of electronic market sub-sets that it had not been exposed to before. Being one of the oldest and most respected electronic component companies in the world, its evolution into circuit protection has been long in coming and we are excited to see another quality vendor in the space.
Paumanok Publications, Inc. estimates the global market for circuit protection components at $5 billion USD in market value worldwide for FY 2016.
KEMET has entered the circuit protection market by pinpointing a specific need in the supply chain to provide automotive grade varistors, which are used for electrostatic discharge protection and overvoltage protection in multiple locations on the automobile (See Figure 2).
To better understand why companies like KEMET are needed for helping major sub-assembly manufacturers such as Robert Bosch, Continental, Nippon Denso, Delphi and Visteon protect their sensitive electronic systems from the unique environments in piston powered and electric vehicles through the application of ceramic based varistors. Automotive companies traditionally prefer using ceramic components because of their reliability during the unique combination of heat and vibration for extended periods of time. The following are circuit applications requiring protection from electrostatic discharge or from an overcurrent event brought about by a load dump (such as jump starting a car).
Driver Comfort, information and Entertainment
There are numerous motor and drive assemblies within an automobile requiring protection from unwanted transients such as the mirror motors, seat motors, sun roof motor, wiper motor and window motors. Paumanok research estimates there are 14 dc motors on average per automobile (sedan and lite truck), with some automobiles having as many as 24 dc motors. (This makes the market for varistors consumed for DC motor protection in the automobile at about 1.3 billion pieces for FY 2016.)
The passenger compartment is also varistor intensive, and includes applications in the air conditioner/climate control systems, stereo system, TV module, buzzers and chimes, and keyless entry. We also include the alarm system and trunk latch control unit in this category for varistor consumption, as well as the tire pressure monitoring system. Additional emerging growth markets in this category include telematics (RF Connectivity), E-Call and tracking devices. The other areas of focused interest are the unique requirements for circuit protection of High Speed Bus Systems (CAN-Controller Area Networks) which allow microcontrollers to operate independently from a host computer inside the car or truck; the high intensity discharge lighting systems (which require higher heat handling components), the camera links, and all touch screen interfaces. (See Figure 2)
Under the Hood Electronics Demand for automotive varistors for use in under-the-hood applications has increased over the past decade to protect various harsh environment electronic systems, units and modules from the affects of tribioelectricity. The major consumer (in dollar value) for varistors are for protection of the engine control units that are application specific to functions of the engine such as ECU’s that control the air/fuel ratio, the idle speed, the variable valve timing, the ignition timing, the revolutions per minute, water temperature, fuel acceleration enrichment, turbocharger waste gate control, as well as specialty engine functions on racing cars. All modern engine control units have a central processing unit that requires circuit protection. Varistors are available in 125° C and 150° C designs to operate effectively in the harsh UTH environment. Additional powertrain applications for varistors include the power steering, engine cooling fan, and transmission controls. (See Figure 2)
Air bag and Restraint Systems
Passenger safety is of primary concern to automotive manufacturers, and these systems are protected from overvoltage transients by varistors. The anti-lock braking system cards, the air bag module, the seat belt tensioner, the parking sensor, the blind spot detection, the radar circuits and lane change assist modules, as well as traction control circuits, electronic suspension, electric brake require varistor protection. (See Figure 2)
In the National Electric Manufacturing Initiative report, Delphi Electronics, one of the world’s largest manufacturers of automotive electronic subassemblies reiterated the need for increased protection for automotive circuits in general purpose and harsh environment applications over the next five to ten years.
Paumanok estimates the global varistor market for automotive electronic subassemblies at approximately $90 million US dollars for FY 2016 with approximately 3 billion varistors consumed in class 3 to 8 cars and trucks. This also translates into 30 varistors per automobile, on average (with about 3.2 million sedans and class 8 trucks produced that require almost twice that number), and this actually translates into approximately $1 dollar in varistor content per car.
Based on my granular analysis of the varistor content per sub-assembly in the automobile, I can make a determination that 1) DRIVER ELECTRONICS is the largest sub-segment in the car and the area with the largest potential growth rate over the next five to ten years. Within the Driver Electronics segment, I can see that the protection of DC motors is a key product sub-market. Almost as lucrative a sub-segment is the 2) UNDER-THE-HOOD markets which require higher heat operation and are more expensive per part, although less parts are required. The engine control units are subjected to a variety of unusual and harsh environment parameters, one of which is the susceptibility of the ECU’s to the affects of electrical transients. And finally, the 3) SAFETY ELECTRONICS segment is also important for varistors, especially for air bag igniters circuits and ABS cards.
The new varistors from KEMET include dual-function varistor-capacitors that combine transient and EMI protection, and plastic-enclosed varistors for increased reliability in humid environments.
The dual-function devices integrate a capacitor to suppress interference from devices such as DC electric motors and are AEC-Q200 qualified. Compact in size, these devices are ideal for protecting sensitive automotive electronics against electric-motor noise as well as potentially damaging high-energy transients. In addition, KEMET has introduced five new surface-mount varistors, including four which are AEC-Q200 qualified. This product line features devices capable of high temperature operation for use in automotive and industrial applications, as well as plastic encapsulations that offer superior humidity resistance.
Figure 2. above also reveals Paumanok’s estimation of where new slots will emerge in the car that will require electrostatic discharge protection. In Driver Electronics we forecast that Heads Up Displays, Telematics, E-Call and CAN Networks will lead the way in a growing field of specific areas within and around the car that need taming, such as lighting, which seems to improve and differentiate at a much faster pace than in commercial or residential lighting. Safety Electronics also hold new slots for circuit protection needed for driver assist circuits, especially radar circuits and proximity sensors.
KEMET’s automotive varistors are available at Mouser Electronics.
Dennis M. Zogbi is the author of more than 260 market research reports on the worldwide electronic components industry. Specializing in capacitors, resistors, inductors and circuit protection component markets, technologies and opportunities; electronic materials including tantalum, ceramics, aluminum, plastics; palladium, ruthenium, nickel, copper, barium, titanium, activated carbon, and conductive polymers. Zogbi produces off-the-shelf market research reports through his wholly owned company, Paumanok Publications, Inc, as well as single client consulting, on-site presentations, due diligence for mergers and acquisitions, and he is the majority owner of Passive Component Industry Magazine LLC.