The Future Needs of Medical Power Supplies in Healthcare
The Medical Power Supply market is experiencing robust growth due to technological advancements, regulatory requirements, increased healthcare spending and home healthcare, expansion in emerging markets, the aging population and the impacts of the COVID-19 pandemic. Current projections place the value of the medical equipment market at an incredible $63 billion with growth predicted to up to 10x that value by 2032 $656 billion. The technological requirements required to support this growth are significant.
From robotic surgery systems and electrosurgical units to life support devices like ventilators, infusion pumps, and defibrillators, medical power supplies are integral. They power equipment such as MRI and CT scanners, ultrasound machines, and X-ray systems. They are crucial for laser surgery systems, heart monitors, blood pressure devices, and home healthcare tools like portable oxygen concentrators and home dialysis equipment. These applications underscore the diverse and vital roles that medical power supplies play in modern healthcare.
To meet these needs, TTI Europe’s range of premium manufacturers of medical power supplies are evolving with new product releases of superior performance, uncompromising reliability, assured safety and compliance, more versatility and with intuitive features.
High efficiency is paramount to reduce heat generation, improve energy usage and provide a reliable power supply. Precise and stable output power is essential for robotic control movements, and low EMI is essential to prevent disruption of sensitive robotic systems.
Effective thermal management is needed to handle the heat generated by high-power medical robotics. Instead of noisy and unreliable fans, alternative methods with either thermal conductive plates or liquid cooling methods are now preferred.
High peak power is necessary in laser applications to deliver intense bursts of energy needed to cut or ablate tissue with precision. Higher peak power also leads to more effective treatments, reducing treatment time and tissue damage and improving overall results of the procedure.
Micro precision is also needed in delicate robotic surgery: peak power enables precise incision and tissue manipulation, improving surgical accuracy and outcomes.
The need for High MTBF (Mean Time Between Failures) will ensure long-term reliability. However, redundancy is also required to ensure continuous operation during power outages and components need to withstand harsh environment and frequent usage. Preventative over voltage, over current and short circuit protection are important to prevent damage to the devices.
Regulatory Approvals must comply with standards like IEC/ UL 60601-1. In addition, patients and operators must be protected from electrical shocks, and very low leakage current is also highly critical to ensure safety.
Multiple Outputs are necessary to be able to provide various voltages required by different parts of the medical systems, and a wide range of input voltages should be considered for different geographical regions. Power supplies may also need to be easily scalable using modular design allowing for easy upgrades or software controlled configurable power supplies.
As the medical world continues to innovate, the demand for advanced, reliable, and efficient medical power supplies will only increase. Meeting these future needs is essential for supporting the next generation of healthcare technology.
If you need design support for your medical power supply, please contact our team of TTI Europe Power Supply Experts. We are here to assist with your design requirements. Please visit here.