To make the TTIEurope.com experience more targeted and user-friendly, TTIEurope.com (and selected third parties) use “cookies” on this website.
This technology helps us gather statistical and analytical information for personalization purposes, but the choice to accept the cookies
is always yours.
Connected car technologies, electric and hybrid vehicle powertrains and the move to more autonomous vehicles are just three of the many trends that are influencing the development of automotive sub-systems. These market requirements are pushing component suppliers to develop improved components that exceed the performance characteristics of previous product generations. TTI actively supports our suppliers by stocking these new products at the earliest possible stage to enable customers to get access and design new applications with the latest automotive approved technologies.
As examples, TTI is supporting Molex to launch its latest Multimedia Modules that enable end users to charge the latest USB handheld devices. We also are working with Vishay and Panasonic to promote their latest power inductors and choke coils as well as focusing on enhanced circuit protection solutions such as diodes from Littelfuse and varistors from TDK and AVX. In addition, the new 200C RHS capacitors from Murata meet the higher temperature requirements for electric vehicle systems.
For more information about our suppliers' solutions, visit www.ttieurope.com.
Best regards,
Dermot Byrne - Director Industry Marketing Transportation
AVX
Automotive Varistors
AVX offers a wide range of AEC-Q200 qualified multilayer varistors designed and manufactured to meet the most stringent circuit protection requirements of modern automotive electronics.
JST
Automotive Connectors - AIT & AIT II Series
JST AIT & AIT II Series 0.64 unsealed low-profile connectors reduce height by over 30% compared to other standard USCAR footprints and can be used in a wide range of automotive applications.
Littelfuse
Automotive Surface Mount Load Dump TVS
The SLD8S TVS automotive series from Littelfuse meets the ISO7637-2 5a/5b protection and ISO16750 load dump test.
Molex
Multimedia Module (CCP)
Off-the-shelf and custom In-Vehicle Charging Modules with smart technology ensure fast battery recharging in a compact and convenient package.
Murata
Lead Type MLCCs for 200°C Automobile Use
Murata Manufacturing Co., Ltd. developed the RHS series of lead type multilayer ceramic capacitors for automobile use at maximum usage temperature of 200°C
Panasonic
Power Inductor Metal Composite Type
Panasonic succeeded in commercializing a Metal Composite power inductor achieving high current characteristic and vibration capability, low power consumption and most important miniaturization.
TDK
Reliable Overvoltage Protection for Automotive Applications
The E Series of CTVS provides reliable overvoltage protection for automotive electronic applications.
EPCOS CTVS® (ceramic transient voltage suppressors) protection devices are based on ceramic multilayer technology.
Vishay
IHLE Series High Current Inductors with E-Field Shield
Vishay expanded its IHLE series of low-profile, high-current inductors featuring integrated e-shields for reduction of EMI with new Automotive Grade devices in the 2525, 3232, and 4040 case sizes.
Yageo
Thin Film Automotive Resistors
Thin film AT series features high precision, high reliability, low TCR, passed Anti-FOS test: ASTM-B-809-95, with robust design for high temperature and moisture resistance.