Pressure Sensors for Residential and Commercial Water Pumps (English)
Booster pumps are a very common way of increasing water pressure in a home or office if the water is coming from a well or if the water pressure coming from the city is low. As the world becomes more conscious of energy use and there are increasing regulations and focus on energy consumption, the OEM’s have moved to variable speed pumps to meet these growing energy concerns.