Power & Storage

Hydrogen Storage

Batteries are not suitable in storing large amounts of electricity over time. A major advantage of hydrogen is that it can be produced from renewable energies, and unlike electricity it can also be stored in large amounts for extended periods of time. For that reason, hydrogen will play an important part in the energy transition.

Electricity Generation

Stationary fuel cells can be used for decentralized power supply in off-grid areas or grid backup systems. In comparison to conventional thermal power plants, fuel cells have much higher electrical efficiencies of up to 60%.

Domestic Energy

If, in addition to the generated electricity, the heat that is produced is also used, the process is referred to as combined heat and power (CHP). Such plants can be used in the domestic heating sector also for smaller outputs.

Applications

  • Building Autom – Heating
  • Stationary Fuel Cells
  • Stationary & Mobile Power Generation
PDF cover for TTI Energy Management Guide
Download this guide to learn more about TTI's Energy Management - Battery Storage & Charging Solutions.

Download: Brochure
powertrain cover
This guide will only focus on in-vehicle applications like Battery Packs, Inverter, E-Motors and On-Board Chargers.

Download: Guide

Featured Suppliers